FB#.IDENTIFIED

Description

This parameter reports the device type that the drive has successfully identified. Its value is based on FB#.SELECT.

Type

Description

0

No feedback identified
1 No Encoder

10

Incremental Encoder with Halls

11

Incremental Encoder without Halls

12

Halls Only

13 Step/Direction
14 CW/CCW

20

Sine Encoder with Halls

21

Sine Encoder without Halls

30

EnDat Analog

31

EnDat Digital

32 BiSS-B Analog
33 HIPERFACE

34

BiSS-C Digital

35 BiSS-B Digital

36

SSI

40

Resolver

41

SFD (Smart Feedback Device)

45 SFD3 (Smart Feedback Device Gen 3)
46 HIPERFACE DSL
47 SFD-M
110 SFA - Incremental Encoder with Halls
111 SFA - Incremental Encoder without Halls

112

SFA - Halls Only

120 SFA - Sine Encoder with Halls
121 SFA - Sine Encoder without Halls
130 SFA - EnDat Analog
131 SFA - EnDat Digital
132 SFA - BiSS-B Analog
133 SFA - HIPERFACE
134 SFA - BiSS-C Digital
135 SFA - BiSS-B Digital
136 SFA - SSI (Synchronous Serial Interface)
140 SFA - Resolver
141 SFA - SFD (Smart Feedback Device)

Versions

Action Version Notes
Implemented 02-00-00-000
Feature Change 02-06-03-000 Added support for SSI feedback.
Feature Change 02-12-01-000 Added BiSS-B Digital types (35, 135).

General Information

Type

Read Only

Units

N/A

Range

N/A

Default Value

N/A

Data Type

Integer

See Also

FB#.SELECT

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Fieldbus Information

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

30000

1

30000 (0x7530)

FB1.IDENTIFIED

Signed16

Read Only

Yes

30001

1

30001 (0x7531)

FB2.IDENTIFIED

Signed16

Read Only

Yes

30002

1

30002 (0x7532)

FB3.IDENTIFIED

Signed16

Read Only

Yes

30003

1

30003 (0x7533)

FB4.IDENTIFIED

Signed16

Read Only

Yes

30004

1

30004 (0x7534)

FB5.IDENTIFIED

Signed16

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

FB1.IDENTIFIED

30000

Signed16

Read Only

-

FB2.IDENTIFIED

30001

Signed16

Read Only

-

FB3.IDENTIFIED

30002

Signed16

Read Only

-

FB4.IDENTIFIED

30003

Signed16

Read Only

-

FB5.IDENTIFIED

30004

Signed16

Read Only

-